| IAグローバル検索 |
...AC G2RV-ST700/500-AP 230 VAC Note: Voltage is reduced within the socket for the slim I/O relay, so the rated input voltage and rated coil voltage of replacement relays are different. Accessor...
...ld be 1 to 5 mm. Note: 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...
...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...
https://www.omron.co.id/products/family/3902/specification.html
...nd the wire 4 turns due to the limitation of the wire size, decrease the number to 3, 2, and so on. When the wire can be wound only a single turn, use 4 or more filters side by side, wi...
https://www.omron.co.id/products/family/3912/specification.html
... Safety Sensors E3ZS OMRON Non-contact Safety Door Switches D40A-2, D40A Safety Output Units NX-SO Unit type Appearance Specifications Unit version Model Number of safety output points Intern...
...before attempting a megger test (insulation resistance measurement) on a Servo Drive. Not doing so may result in the Servo Drive failure. Do not perform a dielectric strength test on the Serv...
https://www.omron.co.id/products/family/3923/specification.html
...value (peak hold), the bottom value (bottom hold), the range of change (peak-to-peak hold), and so forth. Timer mode Allows you to delay upon changes in judgment output, or turn PASS output O...
https://www.omron.co.id/products/family/3932/specification.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
...A switched and 10 A safe switched are from the same source and pass through the same 10 A fuse, so the sum of their current must be less than 10 A. Standards AMR EN IS0 12100, EN ISO 13849-1,...
https://www.omron.co.id/products/family/3950/specification.html
...nnector. *3. However, when bending the cable to perform wiring, maintenance, and other work, do so within the temperature range of 0 to 75°C in consideration of severing of the cable. last up...
https://www.omron.co.id/products/family/871/specification.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron.com.au/products/family/1434/dimension.html
...s, Ltd. --- * There is a risk of quality problems when using cables assembled by typical users, so we recommend purchasing cables with preattached connectors or having a qualified technici...
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.omron.com.au/products/family/1497/specification.html
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.omron.com.au/products/family/1498/specification.html
...V E39-F1V E32-T84SV 1M (No Cutting) E32-T10V 2M (Free Cutting) E32-VF4 Note 1. Mount the Flange so that the V40 O-ring is on the atmospheric-pressure side of the vacuum chamber wall. Note 2. ...
https://www.omron.com.au/products/family/1532/dimension.html
...,000 * HS: 3,450 ST: 4,000 * SHS: 920 E32-LT11R 2M * The optical fiber is 2m long on each side, so the sensing distance is 4,000 mm. Note 1. The following mode names and response times apply ...
...2 Use these small-sized brackets when performing side mounting with standard mounting brackets, so that they do not protrude from the detection surface. 2 for an emitter, 2 for a receiver, to...
... lamp * 100 m 60 m 45 m 30 m Note: Keep the cable length within the rated length. Failure to do so is dangerous as it may prevent safety functions from operating normally. * The F39-...
https://www.omron.com.au/products/family/1581/specification.html
...termined for the current and power that can be provided to the mounted Units. Design the system so that the total current consumption for all the mounted Units does not exceed the maximum tot...
https://www.omron.com.au/products/family/1639/specification.html