| IAグローバル検索 |
...operation is possible for 300-W, 600-W, and 1500-W Power Supplies. *1.Two-conductor shield wire S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...rate - Glossary of Industrial Automation">maximum flowrate, maximum static pressure, and noise. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...of Box Fans are specified for each model. 3. Examples of Inlet-and Outlet-side Fan Installation S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
... due to the voltage applied exceeding the working voltage. Be sure to connect them in parallel. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...ecking the operation or changing filters. Otherwise, contact to the fan blade may cause injury. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...CJT 1 m R87F-PCJT-20 2 m Note:These Plug Cords are for Axial-flow Fans equipped with terminals. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...ight touch a fan blade from the front of the Fan when the panel door is being opened or closed. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...pment that uses a motor to be equipped with a device that protects the motor against overloads. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...s the definition of a Fan's service life. A mechanical illustration of the Axial Fan structure. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...s regularly. (1) Decrease in number of turning (2) Noise increase (3) Abnormal noise generation S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...ime (1 min). In other words, it is the amount of wind that the Fan produces. Unit: Q (m 3 ⁄min) S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...t? Answer Effectiveness is determined by the number and positions of heat-generating objects. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...e Fan is operating in a hypothetical state completely free of resistance. Unit: Qmax (m 3 ⁄min) S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...he Fan is stopped. 2.Static pressure (Ps) is generated at the front of the Fan when it rotates. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...essure in front of the Unit when the front of the fan was completely sealed. Unit: Ps max. (Pa) S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...een the AC Type Axial Fan "R87F" and "R87T"? Answer Refer to the following comparative chart. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...compatibility of EC Directives with the machines and devices that you are using in your system. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
... of them needs to be powered. Applicable models: M7E-08,M7E-12, M7E-20, and M7F Digital Display S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...lect a Power Supply Unit with sufficient capacity for the number of Sensors connected. Example: S8VS-01524 Switch Mode Power Supplies (Input: 100 to 240 VAC, Output: 24 VDC, 0.65 A) S82K-0032...
...es in the output characteristics of products from different companies. Use an OMRON ZCT or ZPD. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...