| IAグローバル検索 |
... parameter, make sure that the current input is not lower than the operating current parameter. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...n using the K2CA-HC Over Current Relay and K2GS-H Earth-fault Directional Relay in combination. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...oles from the same direction. It doesn't matter which wires go through which holes. Tap Setting S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
... the Motor Protective Relay "K2CM Series" or the Multiple Motor Protective Relay "K2MR Series". S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...lectric wires of both terminals to the Heater Element Burnout Detector "K2CU Series" correctly. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...ng values on the overload element, it is recommended to conduct an operating test before using. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...(CT) may be damaged from burning. Location of the Operation Lock Button Side with the Nameplate S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...wn in Figure 2 below is no problem as long as the CT has sufficient capacity. Figure 1 Figure 2 S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...s output to a counter, which makes it possible to easily calculate the total power consumption. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...rect, the power indicator (POWER, green) will flash (see Figure. 3). Figure 1 Figure 2 Figure 3 S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
... (cumulative unit pulse) according to the measured power consumption. Photograph and Dimensions S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
... production quantities (pulses) can be input and unit energy consumption data can be collected. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...consumption is the amount of work per hour. Power W = Voltage (V) × Current (A) × Time (h) [Wh] S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...on is suitable for this kind of application. Applicable models: K2CM, SE Motor Protective Relay S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...to 125%, which satisfies the above standard. Applicable models: K2CM, SE Motor Protective Relay S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...phase Current Transformer. *Input Terminals AGD: K6EL: Z1, Z2 3, 4 Applicable models: AGD, K6EL S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...overload condition extends for a short time. Applicable models: K2CM, SE Motor Protective Relay S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...ecause it is used together with high-voltage equipment, it has K, L indication but no polarity. S8VS Multi-Function Indication Monitor for Production Site Visualization * (* Models with indic...
...2月13日 電源/周邊裝置/其他 電源 電源供應器 S8VK-WA S8VK-WB S8VK-X S8VK-S S8VK-G S8VK-C S8VK-T S8FS-G S8FS-C S8VS S8JX-P S8AS S8AS2 Top of page...
https://www.omron.com.tw/products/family/3485/?recommendation_type=01
...8月24日 電源/周邊裝置/其他 電源 電源供應器 S8VK-WA S8VK-WB S8VK-X S8VK-S S8VK-G S8VK-C S8VK-T S8FS-G S8FS-C S8VS S8JX-P S8AS S8AS2 Top of page...
https://www.omron.com.tw/products/family/3178/?recommendation_type=00