| IAグローバル検索 |
...g position Angle adjustment up to 330° After fastening to the adapter, you can adjust the angle so that the display is easy to see. 180° reverse display The display can rotate 180°. Useful fu...
https://www.omron-ap.co.in/products/family/3720/feature.html
...ction in processing quality. • The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. Solution from OMRON You can use a rise in hyd...
https://www.omron-ap.co.in/products/family/3721/feature.html
...and acts as a beacon to help the robot navigate. The robot uses a Landmark as a reference point so it can better locate objects within the workspace. During high-mix, low-volume production wi...
https://www.omron-ap.co.in/products/family/3739/feature.html
...ase of the shutter. Easy filter replacement The light cover and optical filter are replaceable, so you don't need to prepare a protection cover against dirt. Single camera for inspecting vari...
https://www.omron-ap.co.in/products/family/3740/feature.html
... which allows multiple input voltage ranging 100 to 240 VAC. Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...
https://www.omron-ap.co.in/products/family/3759/feature.html
...te: May 6, 2021 For less design effort DC Axial Fans R89F-DS Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...
https://www.omron-ap.co.in/products/family/3760/feature.html
...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. SOLUTION • You can pickup the product safely with Safely-Limited Spe...
https://www.omron-ap.co.in/products/family/3776/feature.html
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
https://www.omron-ap.co.in/products/family/3779/feature.html
...oducts with safety outputs of which voltage, current, and power are limited to a certain level, so that not to cause an electric shock or fire,” and is evaluated by UL1310. For the UL Class 2...
https://www.omron-ap.co.in/products/family/3780/feature.html
...cements in as little as 10 seconds*1 using e-jig Using e-jig eliminates the need for adjustment so that anyone can install in the same position. Easily upgrade existing facilities to enable “...
https://www.omron-ap.co.in/products/family/3790/feature.html
...ts frequency of automatic measurement allows for understanding the degradation trend, which was so far difficult. K7GE proposes a new way of monitoring insulation. Highly reproducible measure...
https://www.omron-ap.co.in/products/family/3811/feature.html
...etect parts inside the bin. To detect these parts, an operator must reposition items in the bin so that the parts are within the field of view. Cameras installed at the robot arms can reduce ...
https://www.omron-ap.co.in/products/family/3827/feature.html
...arts feeders, roll presses for secondary batteries, assembly machines for digital products, and so on to detect the presence or absence of workpieces. However, many customers are using fiber ...
https://www.omron-ap.co.in/products/family/3831/feature.html
...ate of change of the heater resistance value and monitor the state and tendency of each heater, so it is possible to determine when replacement is necessary, so it is unplanned while...
https://www.omron-ap.co.in/products/family/3855/feature.html
...ifications. Incorrect wiring can lead to failure. *2. Do not connect the shell, for doing so can cause failure or malfunction. *3. When wiring a camera, be sure to refer to its specific...
... documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. last update: October 1, 2024...
... documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. Model Applicable Model General Specifications S-Mount (M12...
...ation documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. Note. STC-M[]S502CXP121/-S[]S510CXP62/-M[]S510CXP121/-M[]S...
... documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. last update: January 5, 2023...
... documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. last update: October 1, 2024...