| IAグローバル検索 |
...ight analog inputs can be connected for each Unit. • There is isolation between input channels, so unwanted circuit paths between thermocouple inputs can be prevented. • Output scaling (±32,0...
https://www.omron-ap.co.th/products/family/1664/feature.html
...ight analog inputs can be connected for each Unit. • There is isolation between input channels, so unwanted circuit paths between thermocouple inputs can be prevented. (Except for CS1W-PTR01/...
https://www.omron-ap.co.th/products/family/1665/feature.html
...e active CPU Unit, the standby CPU Unit takes over in an instant (using the hot standby method) so that system operation continues essentially unaffected. Other duplex variations are also pos...
https://www.omron-ap.co.th/products/family/1684/feature.html
...L, INT, BCD, or STRING. Data configuration files required for the host computer can be created, so necessary data can be retrieved even if the SPU is mounted in a device after the PLC is alre...
https://www.omron-ap.co.th/products/family/1732/feature.html
...nnovative new lock structure makes connection extremely simple. The lock mechanism is internal, so it will no longer become jammed by sputtered fluids or dust. Also, the use of a movable lock...
https://www.omron-ap.co.th/products/family/1827/feature.html
...ous models from OMRON. The protective structure eliminates the need for screws to hold a cover, so there are no worries about loose screws leading to liquid penetration. And the model number ...
https://www.omron-ap.co.th/products/family/1853/feature.html
...s with very few failures. Massive System Variation We provide a wide variety of RFID components so that users can customize configurations for any installation space or objective, from replac...
https://www.omron-ap.co.th/products/family/1863/feature.html
...system, with its highly stable light source, can be turned off when illumination is not needed. So, electricity costs can be reduced. (For a lamp system whose light source is unstable, you ha...
https://www.omron-ap.co.th/products/family/1876/feature.html
...unications baud rate is set without using switches and addresses are set using rotary switches, so setting errors are reduced. • Communications connector and removable I/O terminal block enab...
https://www.omron-ap.co.th/products/family/1919/feature.html
...DC and Low Voltage 24 to 48 VAC/12 to 48 VDC. • ON- and OFF-times can be set independently and so combinations of long ON- or OFF-time and short OFF- or ONtime settings are possible. • Twen...
... design. It offers greater performance and faster I/O response as well as extreme scalability - so you will only need one family. In addition, programming, debugging and networking are faster...
https://www.omron-ap.co.th/products/family/1992/feature.html
... to maintain a stable measurement. They are also susceptible to the influences of ambient light so are difficult to measure using conventional laser measurement sensors. The ZG2 solves these ...
https://www.omron-ap.co.th/products/family/2041/feature.html
...ed for a variety of purposes including dust level setting, alarm output, timed measurement, and so forth. Triggers can be input to initiate monitoring when necessary and alarms can be output ...
https://www.omron-ap.co.th/products/family/2067/feature.html
...nd power factors to appropriate levels. Fixed values are used for the voltage and power factor, so the accuracy specifications do not apply. * Set the voltage to 100 V when performing simple ...
https://www.omron-ap.co.th/products/family/2646/feature.html
... stopped power, standby power, and operating power depending on the power usage conditions so that you can see where energy can be saved. 2) Three-state Energy Classification can be link...
https://www.omron-ap.co.th/products/family/2714/feature.html
...ircuit. Two Outputs: Light-ON and Dark-ON All models provide both a light-ON and dark-ON output so that the output can be switched according to the application simply by changing the wiring. ...
https://www.omron-ap.co.th/products/family/2716/feature.html
... socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Other...
...d I/O signals (12/8 and 0/32). Function blocks up to 128pcs complete this fully flexible range, so you can always be sure of a needs-match solution. Simple Above all, the Omron G9SP range is ...
https://www.omron-ap.co.th/products/family/2937/feature.html
...fe display function The end of the laser diode lifespan is automatically detected and displayed so maintenance can be performed systematically. On the main digital display of the amplifier, t...
https://www.omron-ap.co.th/products/family/2979/feature.html
...even when the door closes slowly. No adhesion of iron particles Permanent magnets are not used, so iron is not attracted, making maintenance easier. Visible safety Checking at the production ...
https://www.omron-ap.co.th/products/family/2989/feature.html