| IAグローバル検索 |
...output frequency, do not use an inverter output as the power source for the Power Supply. Doing so may result in smoking or burning due to internal temperature increases in the Power Supply. ...
https://www.omron-ap.co.th/products/family/3460/specification.html
...is no place to mount the Top-surface Labels on Two-tier Terminal Blocks with a width of 3.5 mm, so they cannot be used. 3. Use commercially available nameplates (9.5 mm wide, 0.5 mm thick) on...
...placement sensor, the measurement point remains the same at any position in the measuring range so that precise measurements can always be made. Measurement in narrow area and by the wall Whe...
https://www.omron-ap.co.th/products/family/3500/feature.html
...llation Example Cut a thread into the workpiece, and screw in the thermocouple while pushing in so that the tip makes complete contact. Note: E52-CA1DF with the same shape and multiple elemen...
https://www.omron-ap.co.th/products/family/3503/specification.html
... Characteristics and Reinforced Insulation for Safety Standard Compliance UL-listed components, so you can reduce the time required for the UL application process. • Using new components or u...
https://www.omron-ap.co.th/products/family/3510/feature.html
...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...
https://www.omron-ap.co.th/products/family/3631/feature.html
...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...
https://www.omron-ap.co.th/products/family/3633/feature.html
...atility and range of Windows programs. The two platforms operate simultaneously but separately, so if Windows is down, the machine just keeps on working. As a result, engineers become unstopp...
https://www.omron-ap.co.th/products/family/3635/feature.html
...in the status which will have an effect on quality and to automatically control the temperature so that the optimal state is always maintained, in the same way as a skilled worker would. This...
https://www.omron-ap.co.th/products/family/3668/feature.html
...in the status which will have an effect on quality and to automatically control the temperature so that the optimal state is always maintained, in the same way as a skilled worker would. This...
https://www.omron-ap.co.th/products/family/3669/feature.html
...d iris adjustment may become loose or come off due to shock or vibration during transportation, so please be caution when unpacking. last update: March 10, 2025...
...d iris adjustment may become loose or come off due to shock or vibration during transportation, so please be caution when unpacking. last update: March 10, 2025...
...g position Angle adjustment up to 330° After fastening to the adapter, you can adjust the angle so that the display is easy to see. 180° reverse display The display can rotate 180°. Useful fu...
https://www.omron-ap.co.th/products/family/3720/feature.html
...ction in processing quality. • The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. Solution from OMRON You can use a rise in hyd...
https://www.omron-ap.co.th/products/family/3721/feature.html
...and acts as a beacon to help the robot navigate. The robot uses a Landmark as a reference point so it can better locate objects within the workspace. During high-mix, low-volume production wi...
https://www.omron-ap.co.th/products/family/3739/feature.html
...ase of the shutter. Easy filter replacement The light cover and optical filter are replaceable, so you don't need to prepare a protection cover against dirt. Single camera for inspecting vari...
https://www.omron-ap.co.th/products/family/3740/feature.html
... which allows multiple input voltage ranging 100 to 240 VAC. Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...
https://www.omron-ap.co.th/products/family/3759/feature.html
...te: May 6, 2021 For less design effort DC Axial Fans R89F-DS Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...
https://www.omron-ap.co.th/products/family/3760/feature.html
...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. SOLUTION • You can pickup the product safely with Safely-Limited Spe...
https://www.omron-ap.co.th/products/family/3776/feature.html
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
https://www.omron-ap.co.th/products/family/3779/feature.html