| IAグローバル検索 |
...ation documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. last update: October 1, 2024...
...nitoring of motors that frequently change speed, which were difficult to identify abnormalities so far. And simplified condition monitoring device parameter configuration process is contribut...
...t and accurate collection of high‐resolution data in chronological order, the amount of data is so large that the data transfer to databases becomes a bottleneck. [NX5] With approximately fou...
...d in continuous or strobed mode. NERLITE Smart Series Lights have a built-in strobe controller, so no external strobe controller is needed. Dedicated cable sets allow you to wire the NERLITE ...
...t having to take a robot out of production. The onscreen display includes a virtual robot stick so users can control the robot just as they would control a physical robot. In addition to the ...
...imed STO. The torque in the motor is removed at a certain (settable) time after SS1 activation, so the controller has time to stop the load in a controlled manner before the STO is executed. ...
...ngle characteristics of ±85° max. Place the sensors away from the pathways of people and robots so that the sensors do not obstruct their movement. Thus remove failure risks such as optical a...
...ror displayed in multiple languages [PATENT PENDING] *1 ZP-L’s display supports four languages, so that on-site workers at local factories can understand its configuration. Error displays hav...
...nutes to seconds Result of Learn • Tools arranged in reading order • ROIs (Regions of Interest) so each code can be read uniquely • ROI sized to accommodate the expected positional uncertaint...
...etup completed in just a few minutes Intuitive UI for effortless use The AI Detection Camera is so intuitive that even first-time users can set it up. Just follow the on-screen steps and conf...
...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...
...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...
...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...
... socket. When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards (see the figure below). Other...
... now be connected with a short bar in the G70D-SOC08. • No tools are required to remove Relays, so Relay replacement is easier than ever. • The attached terminal cover prevents shocks. • Equi...
...• The Configurator can be used to calibrate temperatures. • The circuit section can be removed, so rewiring isn’t required during maintenance. • DIN track mounting. last update: December 19, ...
...inescent color of the LED. The materials used for the IP40 and oil-resistant IP66 are different so be sure to use a Color Cap that matches the specifications of the Switch. • Not all combinat...
... be replaced during power supply or operation. In addition, cable disconnections are monitored, so failures can be located easily. Remove or add units without using a programming device The d...
...DS10T-V. Meanwhile, the ZX-TDS10T-VL can control air push models in addition to air lift models so that contact force can now be controlled externally. Combines Reliability and Innovations in...
...he 0.5-m type, a repeat accuracy of 1 mm or better has been achieved. The Sensor is ultrasonic, so it is not affected by the color of objects. A variety of materials can be measured, includin...