Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 5121 - 514025803
E3NC Smart Laser Sensors/Features | OMRON Industri...

... have a single wavelength. With high-frequency Modulation, the emitted laser beam is controlled so that it contains multiple wavelengths. Diffuse-reflective Model E3NC-LH02 Long-distance and ...

https://www.omron.com.au/products/family/3316/feature.html

NJ501-4[][][] NJ-series NJ Robotics CPU Units/Feat...

... Reuse of codes • The 3D simulation is very reliable since it is based on the real system cores so you can reuse the whole programming to control the real machine by significantly shortening ...

https://www.omron.com.au/products/family/3387/feature.html

E3S-DB Transparent Object Detection Photoelectric ...

...w beam diameter of minimum 2.5 mm The E3S-DB has a response time of 0.5 ms for a pitch of 5 mm, so detection is possible at a conveyor speed of up to 4 m/s. (With the E3S-DB[][]2(T) and a sen...

https://www.omron.com.au/products/family/3455/feature.html

S8FS-C Switch Mode Power Supply (15/25/35/50/75/10...

...output frequency, do not use an inverter output as the power source for the Power Supply. Doing so may result in smoking or burning due to internal temperature increases in the Power Supply. ...

https://www.omron.com.au/products/family/3460/specification.html

XW5T-P DIN Track Push-in Terminal Blocks/Lineup | ...

...is no place to mount the Top-surface Labels on Two-tier Terminal Blocks with a width of 3.5 mm, so they cannot be used. 3. Use commercially available nameplates (9.5 mm wide, 0.5 mm thick) on...

https://www.omron.com.au/products/family/3480/lineup.html

ZW-8000 / 7000 / 5000 Series Confocal Fiber Displa...

...placement sensor, the measurement point remains the same at any position in the measuring range so that precise measurements can always be made. Measurement in narrow area and by the wall Whe...

https://www.omron.com.au/products/family/3500/feature.html

E52 with Ferrule (Low-cost Models) Temperature Sen...

...llation Example Cut a thread into the workpiece, and screw in the thermocouple while pushing in so that the tip makes complete contact. Note: E52-CA1DF with the same shape and multiple elemen...

https://www.omron.com.au/products/family/3503/specification.html

G3PJ Solid State Relays for Heaters/Features | OMR...

... Characteristics and Reinforced Insulation for Safety Standard Compliance UL-listed components, so you can reduce the time required for the UL application process. • Using new components or u...

https://www.omron.com.au/products/family/3510/feature.html

NYB Industrial PC Platform NY-series Industrial Bo...

...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...

https://www.omron.com.au/products/family/3631/feature.html

NYP Industrial PC Platform NY-series Industrial Pa...

...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...

https://www.omron.com.au/products/family/3633/feature.html

NY5[][]-1 Industrial PC Platform NY-series IPC Mac...

...atility and range of Windows programs. The two platforms operate simultaneously but separately, so if Windows is down, the machine just keeps on working. As a result, engineers become unstopp...

https://www.omron.com.au/products/family/3635/feature.html

E5CD / E5CD-B Digital Temperature Controller (48 x...

...in the status which will have an effect on quality and to automatically control the temperature so that the optimal state is always maintained, in the same way as a skilled worker would. This...

https://www.omron.com.au/products/family/3668/feature.html

E5ED / E5ED-B Digital Temperature Controller (48 x...

...in the status which will have an effect on quality and to automatically control the temperature so that the optimal state is always maintained, in the same way as a skilled worker would. This...

https://www.omron.com.au/products/family/3669/feature.html

3Z4S-LE VS-LLD Series Ultra-high-resolution Lens f...

...d iris adjustment may become loose or come off due to shock or vibration during transportation, so please be caution when unpacking. last update: March 10, 2025...

https://www.omron.com.au/products/family/3691/lineup.html

3Z4S-LE VS-TEV Series Ultra-high-resolution Telece...

...d iris adjustment may become loose or come off due to shock or vibration during transportation, so please be caution when unpacking. last update: March 10, 2025...

https://www.omron.com.au/products/family/3692/lineup.html

E8FC IoT Flow Sensors/Features | OMRON Industrial ...

...g position Angle adjustment up to 330° After fastening to the adapter, you can adjust the angle so that the display is easy to see. 180° reverse display The display can rotate 180°. Useful fu...

https://www.omron.com.au/products/family/3720/feature.html

E8PC IoT Pressure Sensors/Features | OMRON Industr...

...ction in processing quality. • The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. Solution from OMRON You can use a rise in hyd...

https://www.omron.com.au/products/family/3721/feature.html

TM Series Collaborative Robots/Features | OMRON In...

...and acts as a beacon to help the robot navigate. The robot uses a Landmark as a reference point so it can better locate objects within the workspace. During high-mix, low-volume production wi...

https://www.omron.com.au/products/family/3739/feature.html

FHV7 Series Smart Camera/Features | OMRON Industri...

...ase of the shutter. Easy filter replacement The light cover and optical filter are replaceable, so you don't need to prepare a protection cover against dirt. Single camera for inspecting vari...

https://www.omron.com.au/products/family/3740/feature.html

R89F-M AC Free Input Axial Fans/Features | OMRON I...

... which allows multiple input voltage ranging 100 to 240 VAC. Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...

https://www.omron.com.au/products/family/3759/feature.html

結果 5121 - 514025803

国/地域選択

Related Contents