Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 5181 - 520025803
CS1W-PTS SYSMAC CS-series Process Analog I/O Units...

...ight analog inputs can be connected for each Unit. • There is isolation between input channels, so unwanted circuit paths between thermocouple inputs can be prevented. • Output scaling (±32,0...

https://www.omron.com.vn/products/family/1664/feature.html

CS1W-PDC / PTW / PTR SYSMAC CS-series Process Anal...

...ight analog inputs can be connected for each Unit. • There is isolation between input channels, so unwanted circuit paths between thermocouple inputs can be prevented. (Except for CS1W-PTR01/...

https://www.omron.com.vn/products/family/1665/feature.html

CS1W-LCB01 / LCB05 Loop Control Boards/Features | ...

...e active CPU Unit, the standby CPU Unit takes over in an instant (using the hot standby method) so that system operation continues essentially unaffected. Other duplex variations are also pos...

https://www.omron.com.vn/products/family/1684/feature.html

CJ1W-SPU01-V2 CJ-series High-speed Data Storage Un...

...L, INT, BCD, or STRING. Data configuration files required for the host computer can be created, so necessary data can be retrieved even if the SPU is mounted in a device after the PLC is alre...

https://www.omron.com.vn/products/family/1732/feature.html

XS5 Round Water-resistant Connectors (M12 Smartcli...

...nnovative new lock structure makes connection extremely simple. The lock mechanism is internal, so it will no longer become jammed by sputtered fluids or dust. Also, the use of a movable lock...

https://www.omron.com.vn/products/family/1827/feature.html

E3ZM-C Oil-resistant, Robust, Compact Photoelectri...

...ous models from OMRON. The protective structure eliminates the need for screws to hold a cover, so there are no worries about loose screws leading to liquid penetration. And the model number ...

https://www.omron.com.vn/products/family/1853/feature.html

V680 Series RFID System/Features | OMRON Industria...

...s with very few failures. Massive System Variation We provide a wide variety of RFID components so that users can customize configurations for any installation space or objective, from replac...

https://www.omron.com.vn/products/family/1863/feature.html

ZUV-C20H / 30H Smart Curing System (Standard model...

...system, with its highly stable light source, can be turned off when illumination is not needed. So, electricity costs can be reduced. (For a lamp system whose light source is unstable, you ha...

https://www.omron.com.vn/products/family/1876/feature.html

CRT1-[]D08TA(-1) / []D16TA(-1) / []D08TAH(-1) / []...

...unications baud rate is set without using switches and addresses are set using rotary switches, so setting errors are reduced. • Communications connector and removable I/O terminal block enab...

https://www.omron.com.vn/products/family/1919/feature.html

H3CR-F Solid-state Timer/Features | OMRON Industri...

...DC and Low Voltage 24 to 48 VAC/12 to 48 VDC.  • ON- and OFF-times can be set independently and so combinations of long ON- or OFF-time and short OFF- or ONtime settings are possible.  • Twen...

https://www.omron.com.vn/products/family/194/feature.html

CJ2 CJ2 Overview/Features | OMRON Industrial Autom...

... design. It offers greater performance and faster I/O response as well as extreme scalability - so you will only need one family. In addition, programming, debugging and networking are faster...

https://www.omron.com.vn/products/family/1992/feature.html

ZG2 Smart Sensor (2D Measurement Sensor)/Features ...

... to maintain a stable measurement. They are also susceptible to the influences of ambient light so are difficult to measure using conventional laser measurement sensors. The ZG2 solves these ...

https://www.omron.com.vn/products/family/2041/feature.html

ZN-PD-S Air Particle Sensor/Features | OMRON Indus...

...ed for a variety of purposes including dust level setting, alarm output, timed measurement, and so forth. Triggers can be input to initiate monitoring when necessary and alarms can be output ...

https://www.omron.com.vn/products/family/2067/feature.html

KM50-C Smart Power Monitor/Features | OMRON Indust...

...nd power factors to appropriate levels. Fixed values are used for the voltage and power factor, so the accuracy specifications do not apply. * Set the voltage to 100 V when performing simple ...

https://www.omron.com.vn/products/family/2646/feature.html

KM50-E Smart Power Monitor/Features | OMRON Indust...

... stopped power, standby power, and      operating power depending on the power usage conditions so that you can see where energy can be saved. 2) Three-state Energy Classification can be link...

https://www.omron.com.vn/products/family/2714/feature.html

EE-SX97 Slot-type Photomicrosensor/Features | OMRO...

...ircuit. Two Outputs: Light-ON and Dark-ON All models provide both a light-ON and dark-ON output so that the output can be switched according to the application simply by changing the wiring. ...

https://www.omron.com.vn/products/family/2716/feature.html

G3R-I/O I/O Solid State Relays/Lineup | OMRON Indu...

... socket.              When using the short bars on the upper section of the socket, insert them so that their heads are pointed upwards              (see the figure below).              Other...

https://www.omron.com.vn/products/family/2808/lineup.html

G9SP Safety Controller/Features | OMRON Industrial...

...d I/O signals (12/8 and 0/32). Function blocks up to 128pcs complete this fully flexible range, so you can always be sure of a needs-match solution. Simple Above all, the Omron G9SP range is ...

https://www.omron.com.vn/products/family/2937/feature.html

ZX2 Smart Sensors Laser Displacement Sensors CMOS ...

...fe display function The end of the laser diode lifespan is automatically detected and displayed so maintenance can be performed systematically. On the main digital display of the amplifier, t...

https://www.omron.com.vn/products/family/2979/feature.html

D40Z Compact non-contact Door Switch/Features | OM...

...even when the door closes slowly. No adhesion of iron particles Permanent magnets are not used, so iron is not attracted, making maintenance easier. Visible safety Checking at the production ...

https://www.omron.com.vn/products/family/2989/feature.html

結果 5181 - 520025803

国/地域選択

Related Contents