| IAグローバル検索 |
...4 mm mounting hole pitch as well as the E3AS Sensors. The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
https://www.fa.omron.co.jp/data_pdf/cat/e3as-hl_f_l_e594-e1_4_7_csm1105100.pdf
...e to be selected each time the shape, color, pattern, or reflectivity of the workpiece changes, so the equipment sometimes need to be redesigned. The E3AS Series can detect workpieces without...
https://www.fa.omron.co.jp/data_pdf/cat/e3as-hl_f_l_e595-e1_10_1_csm1105104.pdf
...gh power density. (Applicable to the E3C-LD11N/E3C-LR11N) Do not disassemble the product. Doing so may cause the laser beam to leak, resulting in the danger of visual impairment. (Applicable ...
https://www.fa.omron.co.jp/data_pdf/cat/e3c-lda_n_e605-e1_1_3_csm1118673.pdf
...e Slit to the upper indented mounting portion of the Sensor and adjust the position of the Slit so that the Slit will be in parallel to the lens side of the Sensor. 1 2 2. Press the lower pro...
https://www.fa.omron.co.jp/data_pdf/cat/e3c_photoelectric_operation_tg_e_7_3_csm442.pdf
...ed herein may result in hazardous radiation exposure. Do not disassemble the Sensor Head. Doing so may cause the laser beam to leak, resulting in a risk of visual impairment. • The following ...
https://www.fa.omron.co.jp/data_pdf/cat/e3nc_ds_e_9_6_csm1018967.pdf
... have a single wavelength. With high-frequency Modulation, the emitted laser beam is controlled so that it contains multiple wavelengths. Emitted wavelength Conventional Transparent O Object ...
https://www.fa.omron.co.jp/data_pdf/cat/e3nc_e427-e1_10_1_csm1010501.pdf
...ossible with the current distributed placement without increasing the cost.There is less wiring so wiring cost and work are also reduced. Commissioning systems overseas and reconnection by th...
https://www.fa.omron.co.jp/data_pdf/cat/e3nw_e428-e1_4_5_csm1012349.pdf
...nt level The incident light level difference is 4,000 when the level is 5,000 with a workpiece, so a threshold of 3,000 is OK. The passing time is "13 ms", so it is OK with Standard ...
https://www.fa.omron.co.jp/data_pdf/cat/e3nx-fa_e426-e1_10_5_csm1010499.pdf
... time incident level ST Difference in incident level The difference in incident level is large, so use B. 4 L O U T 13a 4000 D DPC Passing time The passing time is "13 ms", so it is ...
https://www.fa.omron.co.jp/data_pdf/cat/e3nx-ma_e466-e1_1_4_csm1060634.pdf
...32-LD11 2M 820 330 250 74 E32-LD11R 2M 790 310 240 71 *1. The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Sensing directi...
https://www.fa.omron.co.jp/data_pdf/cat/e3nx-ma_e467-e1_1_7_csm1060689.pdf
...es may become immersed in oil or other liquids or where liquids may penetrate the Sensor. Doing so may result in damage from burning and fire, particularly if the liquid is flammable. 3. When...
https://www.fa.omron.co.jp/data_pdf/cat/e3s-a_ds_e_13_1_csm1296.pdf
... must be 1.18 N·m maximum. Mounting Bracket • When mounting the E3S-C with the mounting bracket so that sensing objects will be in the direction of the mechanical axis, use the optical axis l...
https://www.fa.omron.co.jp/data_pdf/cat/e3s-c_ds_e_9_4_csm424.pdf
...ty Precautions Refer to Warranty and Limitations of Liability. WARNING • Also, mount the Sensor so that it is not aligned with extreme changes in color or materials, as shown below. This prod...
https://www.fa.omron.co.jp/data_pdf/cat/e3s-cl_ds_e_5_5_csm425.pdf
...e used. These Photoelectric Sensors can stably With the E3S-DB detect transparent glass bottles so that you can increase equipment operating rates. New technology Reflector E39-R1S This Is Ho...
https://www.fa.omron.co.jp/data_pdf/cat/e3s-db_e440-e1_6_1_csm1042707.pdf
...ions for Safe Use The following precautions must be observed to ensure safe operation. 1. Doing so may cause damage or fire. Do not install the product in the following locations. • Locations...
https://www.fa.omron.co.jp/data_pdf/cat/e3s-r_ds_e_10_5_csm428.pdf
...surface, the E3SR may not detect it properly. To avoid this situation, place the sensing object so that it is not at right angles to the Photoelectric Sensor. Reflector Precautions for Safe U...
https://www.fa.omron.co.jp/data_pdf/cat/e3s_ds_e_13_2_csm1308.pdf
...Mounting When mounting the Sensor, never strike it with a heavy object, such as a hammer. Doing so may reduce its watertight properties. Use screws with spring, flat, or toothed washers to se...
https://www.fa.omron.co.jp/data_pdf/cat/e3t_e407-e1_6_8_csm2648.pdf
...0 4,000 * 2,000 4,000 * 4,000 * 110 290 840 780 840 140 * The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Sensing distance (mm) High-speed Standard mode mo...
https://www.fa.omron.co.jp/data_pdf/cat/e3x-hd_ds_e_7_5_csm1012032.pdf
...on’s proprietory Smart Power Control combines APC and DPC to automatically compensate the power so that high-precision detection with no maintenance is performed. And if compensation is not p...
https://www.fa.omron.co.jp/data_pdf/cat/e3x-hd_e417-e1_5_2_csm1001626.pdf
...16 Reflective Top-view 4° E32-D16 2M Integrated lens *1. The fiber length is 10 m on each side, so the sensing distance is given as 20,000 mm. *2. The fiber length is 2 m on each side, ...
https://www.fa.omron.co.jp/data_pdf/cat/e3x-sd_na_e401-e1_6_4_csm2185.pdf