Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 9041 - 906025803
PDFIO-Link AD Converter K3CV Analog signals are conve...

...r use this product with AC power supply or with voltage in excess of the rated voltage as doing so may result in rupturing or fire. CAUTION This product cannot be used in explosion hazard are...

https://www.fa.omron.co.jp/data_pdf/cat/k3cv_h243-e1_4_1_csm1132260.pdf

PDF[-] K3GN Data Sheet

...tting the scaling display value. Note: When pulse input is used, the base point is the 0 point, so the settings are only the input value and the display value. Displayed value Displayed value...

https://www.fa.omron.co.jp/data_pdf/cat/k3gn_ds_e_7_2_csm253.pdf

PDFUp/Down Counting Pulse Indicator

....5 m) ÷ 250 = 2. 1. The prescale value for the K3HB-C is set using the mantissa X × exponent Y, so the prescale value = 2.0000 × 10°, X = 2.000, and Y = 00. 2. Next, set the decimal point pos...

https://www.fa.omron.co.jp/data_pdf/cat/k3hb-c_ds_e_17_6_csm259.pdf

PDFTemperature Indicator K3HB-H CSM_K3HB-H_DS_E_14_7

...of the derating area (i.e., do not use it in the area labeled (1) in the above graphics). Doing so may occasionally cause deterioration or damage to internal components. Component Names and ...

https://www.fa.omron.co.jp/data_pdf/cat/k3hb-h_ds_e_14_7_csm260.pdf

PDFTimer Interval Indicator K3HB-P CSM_K3HB-P_DS_E_16...

...nditions with the standard mounting. The derating curve will vary with the mounting conditions, so be sure to adjust accordingly. 2. Internal components may be deteriorated or damaged. Do not...

https://www.fa.omron.co.jp/data_pdf/cat/k3hb-p_ds_e_16_6_csm261.pdf

PDFRotary Pulse Indicator K3HB-R CSM_K3HB-R_DS_E_16_6

...nditions with the standard mounting. The derating curve will vary with the mounting conditions, so be sure to adjust accordingly. 2. Internal components may be deteriorated or damaged. Do not...

https://www.fa.omron.co.jp/data_pdf/cat/k3hb-r_ds_e_16_6_csm262.pdf

PDFLinear Sensor Indicator K3HB-S CSM_K3HB-S_DS_E_11_...

...of the derating area (i.e., do not use it in the area labeled (1) in the above graphics). Doing so may occasionally cause deterioration or damage to internal components. „Component Names and ...

https://www.fa.omron.co.jp/data_pdf/cat/k3hb-s_ds_e_11_7_csm263.pdf

PDFWeighing Indicator K3HB-V CSM_K3HB-V_DS_E_11_7

...of the derating area (i.e., do not use it in the area labeled (1) in the above graphics). Doing so may occasionally cause deterioration or damage to internal components. „Component Names and ...

https://www.fa.omron.co.jp/data_pdf/cat/k3hb-v_ds_e_11_7_csm264.pdf

PDFProcess Indicator K3HB-X CSM_K3HB-X_DS_E_12_7

...of the derating area (i.e., do not use it in the area labeled (1) in the above graphics). Doing so may occasionally cause deterioration or damage to internal components. Component Names and ...

https://www.fa.omron.co.jp/data_pdf/cat/k3hb-x_ds_e_12_7_csm254.pdf

PDF[-] K3MA-F Data Sheet

...ating environment, deterioration, contraction, or hardening of the rubber packing may occur and so, in order to ensure the level of waterproofing specified in NEMA TYPE 4, periodic replacemen...

https://www.fa.omron.co.jp/data_pdf/cat/k3ma-f_ds_e_14_4_csm265.pdf

PDF[-] K3MA-J Data Sheet

...ating environment, deterioration, contraction, or hardening of the rubber packing may occur and so, in order to ensure the level of waterproofing specified in NEMA TYPE 4, periodic replacemen...

https://www.fa.omron.co.jp/data_pdf/cat/k3ma-j_ds_e_13_5_csm255.pdf

PDF[-] K3MA-L Data Sheet

...ating environment, deterioration, contraction, or hardening of the rubber packing may occur and so, in order to ensure the level of waterproofing specified in NEMA TYPE 4, periodic replacemen...

https://www.fa.omron.co.jp/data_pdf/cat/k3ma-l_ds_e_11_4_csm266.pdf

PDF[N218-E1-08] K6CM Data Sheet (Including K6CM-CIM, ...

...ns and then use them, the value of acceleration and the value of velocity will be inconsistent, so measurement cannot be correctly monitored. (01)04549734178730 (21)1342177281 MES:Ver.1.0 (01...

https://www.fa.omron.co.jp/data_pdf/cat/k6cm_n218-e1_3_1_csm1060693.pdf

PDFMotor Condition Monitoring Device

...chment is used. *6. Even if the motor is not moving, the value of velocity may appear slightly, so that the measurement value is fixed at 0.00 mm/s until the value reaches 0.90 mm/s or higher...

https://www.fa.omron.co.jp/data_pdf/cat/k6cm_n218-e1_5_4_csm1060693.pdf

PDF[N220-E1-09] K6CM series Catalog

...omatically set the threshold by entering the Motor shaft diameter, Rotation speed, capacity and so on. Trend Monitoring You can check the trend of the measured values in a graph on the screen...

https://www.fa.omron.co.jp/data_pdf/cat/k6cm_n220-e1_2_1_csm1060685.pdf

PDF[N223-E1-02] K6CM Series Application Guide

...al) 50 Expected implementation effects Detects air locks in pumps and other abnormal conditions so that the system can be maintained before degradation causes it to shut down. 5 I. Pump syste...

https://www.fa.omron.co.jp/data_pdf/cat/k6cm_n223-e1-02.pdf

PDF[N234-E1-05] K7DD Data Sheet

... press the hook firmly until you hear it lock into place. • Do not ground the special CT. Doing so may result in malfunction. 10 (example: motor side) Load side (L) (example: inverter or driv...

https://www.fa.omron.co.jp/data_pdf/cat/k7dd_n234-e1_3_3_csm1124083.pdf

PDF[N235-E1-04] K7DD Catalog

... of Condition Based Maintenance Reactive maintenance has been the standard maintenance strategy so far, due to a limitation of skilled resources. The severe labor shortages seen in recent yea...

https://www.fa.omron.co.jp/data_pdf/cat/k7dd_n235-e1_2_1_csm1124086.pdf

PDF[N225-E1-06] K7GE-MG Data Sheet

...t any other device such as a transformer or a filter between the contactor and the motor. Doing so may cause incorrect measurement. R S T Contactor MC-a Connect the voltage input of the Probe...

https://www.fa.omron.co.jp/data_pdf/cat/k7ge-mg_n225-e1_2_2_csm1106906.pdf

PDF[N226-E1-04] K7GE Catalog

...ts frequency of automatic measurement allows for understanding the degradation trend, which was so far difficult. K7GE proposes a new way of monitoring insulation. Solution 1 Highly reproduci...

https://www.fa.omron.co.jp/data_pdf/cat/k7ge_n226-e1_2_2_csm1107457.pdf

結果 9041 - 906025803

国/地域選択

Related Contents