| IAグローバル検索 |
...scraps or dust to enter the mating section. Cable Lead Polarity • Wire as in the wiring diagram so that the polarities of cable cores (blue: negative power supply, brown: positive power suppl...
https://www.fa.omron.co.jp/data_pdf/cat/xw3d_ds_e_3_5_csm1341.pdf
...rotective Covers cannot be used with a Capactive Proximity Sensor.] The cover uses Fluororesin, so that chips that adhere due to sputtering can be easily removed. Sputter Protective Cover Dim...
https://www.fa.omron.co.jp/data_pdf/cat/y92__ds_e_7_4_csm470.pdf
...at a stable level in a large amount of ambient light, even on objects that do not reflect light so much such as black ones. Measurement performance margin for transparent objects and glossy o...
https://www.fa.omron.co.jp/data_pdf/cat/zg2_q167-e1_6_8_csm2085.pdf
...Do not use the Power Monitor in locations where flammable or explosive gases are present. Doing so may occasionally result in minor or moderate explosion, causing minor or moderate injury, or...
https://www.fa.omron.co.jp/data_pdf/cat/zn-ctc11_ds_e_2_1_csm1013052.pdf
...error displayed in multiple languages PATENT PENDING *1 ZP-L’s display supports four languages, so that on-site workers at local factories can understand its configuration. Error displays hav...
https://www.fa.omron.co.jp/data_pdf/cat/zp-l_q362-e1_4_1_csm1130069.pdf
...h power density and exposure may result in loss of sight. Do not disassemble the product. Doing so may cause the laser beam to leak, resulting in the danger of visual impairment. For details,...
https://www.fa.omron.co.jp/data_pdf/cat/zs-n_ds_e_7_2_csm1012042.pdf
...s to the next pixel when excessive light is received. This phenomenon does not occur with CMOS, so there are no effects from light fluctuations from different materials or excessive light rec...
https://www.fa.omron.co.jp/data_pdf/cat/zs_e375-e1_5_12_csm1393.pdf
...ng System ZUV Series The UV Curing System Value Model Controllers New UV LEDs Value Model Heads So, will you keep on using a lamp system ? Cost performance that will overwhelm a lamp system A...
https://www.fa.omron.co.jp/data_pdf/cat/zuv_e364-e1_10_2_csm1003337.pdf
...yourself may cause danger. 9. Do not attempt to dismantle, repair, or modify the product. Doing so may cause the product to not operate correctly as well as cause a malfunction resulting in a...
https://www.fa.omron.co.jp/data_pdf/cat/zuv_e607-e1_1_1_csm1119254.pdf
...ocal office or sales office. 9. Do not try to disassemble, repair, or modify the product. Doing so may result in malfunctions, causing fire or electric shock. 10. Dispose this product as indu...
https://www.fa.omron.co.jp/data_pdf/cat/zuv_series_ds_e_8_3_csm1012207.pdf
...ng the same axis, the measurement point remains the same at any position in the measuring range so that precise measurements can always be achieved. 5 Smallest in class *6 Ultra-small head Co...
https://www.fa.omron.co.jp/data_pdf/cat/zw-8000_7000_5000_q250-e1_6_15_csm1050134.pdf
... power equipment. ■ Wiring Do not use the product at voltages exceeding the rated values. Doing so may result in damage. Do not connect the product to an AC power supply or connect the power ...
https://www.fa.omron.co.jp/data_pdf/cat/zx-e_e331-e1_8_2_csm1398.pdf
...-GTC41 DC Accessories (Order Separately) These are not included with the sensor and controller, so order these accessories separately if necessary. Set: Interface Unit (RS-232C/Binary output)...
https://www.fa.omron.co.jp/data_pdf/cat/zx-gt_ds_e_1_5_csm1738.pdf
... If the Unit must be used without terminating the laser beam path, position the laser beam path so that it is not at eye level. 3. To avoid exposure to hazardous laser radiation, do not displ...
https://www.fa.omron.co.jp/data_pdf/cat/zx-l-n_e349-e1_1_13_csm2061.pdf
...ements Do not expose the plunger to forces exceeding the limits in the following diagram. Doing so may damage the plunger. ZX-TDS-Series Sensors • The Sensor may be destroyed if excessive for...
https://www.fa.omron.co.jp/data_pdf/cat/zx-t_e345-e1_2_3_csm1741.pdf
...cified herein may result in hazardous radiation exposure. Do not disassemble the product. Doing so may cause the laser beam to leak, resulting in the danger of visual impairment. Note: For Pr...
https://www.fa.omron.co.jp/data_pdf/cat/zx0_e444-e1_4_1_csm1012044.pdf
...ithin 200 ms ON OFF Signal Laser emission reception OFF 4 Do not disassemble the product. Doing so may cause the laser beam to leak, resulting in the danger of visual impairment. Note: For Pr...
https://www.fa.omron.co.jp/data_pdf/cat/zx1_e416-e1_5_5_csm1001847.pdf
...05 48 Measurement center distance (43.85) workpiece (19.85) 10.5° ±0.1° Adjust the installation so that the angle is 10.5° ±0.1°. * The mounting hole dimensions in parentheses (reference valu...
https://www.fa.omron.co.jp/data_pdf/cat/zx2_ds_e_6_7_csm2680.pdf
...fe display function The end of the laser diode lifespan is automatically detected and displayed so maintenance can be performed systematically. On the main digital display of the amplifier, t...
https://www.fa.omron.co.jp/data_pdf/cat/zx2_e406-e1_15_1_csm2639.pdf
...LED LED G R X Ta 電源回路 X1C 電源回路 Z21 B2 P0 Tc Tb 衝撃波吸収回路 B1 RY10/a F P1 Ta So Tc 吸衝収撃回波路 注. 形AGS-Hにはブザーは内蔵となっています。 お願い B1、B2端子にはAC100Vが出力され...