Page top

Lead Contents

FAQ02285 of Safety Sensors FAQ

FAQ No. FAQ02285

Primary Contents

Question

Why does the Short-range Safety Light Curtain "F3SN/F3SH" employ the PNP output?

Answer



In the case when equipment is connected to a common earth ground (0V), the PNP output is used to prevent an output malfunction due to earth fault.

Therefore, Safety Sensors/ Safety Light Curtains designed for safe use employ the PNP output for ensuring the safety of customers.

Earth fault

* If the side of 24VDC is grounded, safety is ensured.

When using the NPN output, if a coating of output lines peels off and they are touching the frame of facilities, a hazardous source keeps existing and uncontrollable. It is very dangerous. Burnout of the coating and short circuit to the frame occur at an extremely high ratio.

Earth fault

If output lines are short-circuited, loads are stopped without running away because any voltage is not applied to them. It is very safe.

Reference

However, the system connected to 24VDC ground can also use equipment with NPN output, thus NPN output type models are also available for the F3SN-B Series.

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Sensors FAQ