Page top

Lead Contents

FAQ02361 of Safety Sensors FAQ

FAQ No. FAQ02361

Primary Contents

Question

What is the protective height?

Answer



The protective height is the range in which an object can be detected.

With F3SN-A-series Safety Light Curtains and F3SN-B-series, extra space can be minimized by making the protective height and sensor length the same, as shown in the following diagram.

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Sensors FAQ