Page top

Lead Contents

FAQ02365 of Safety Sensors FAQ

FAQ No. FAQ02365

Primary Contents


What is the smallest detectable object for F3SN series Safety Light Curtain?


The smallest detectable object is one of a size that will always break the Safety Light Curtain beam at any point in the Safety Light Curtain protective height.

Specifically, the smallest detectable object is a non-transparent object as big as the optical axis pitch plus the lens diameter, as shown in the following diagram that will break the beam at any point (position).

F3SN-A[][][][]P14 (Optical axis pitch: 9 mm, Smallest detectable object: 14 mm dia.)

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Sensors FAQ