Page top

Lead Contents

FAQ02164 of Thumbwheel Switches FAQ

FAQ No. FAQ02164

Primary Contents

Question

Is it possible to display only "+" and "-"?

Answer



Yes, it is.

Models with binary-coded decimal (06 models) are available that display "+, -, +, -. . ." rather than "0, 1, 2, 3, 4, 5 . . . 9".

The models are the A7[]-206-PM and A7[]-206-PM-1.

Example:

Thumbwheel Switch
A7BS-206-PM

Output Code:

The signal between output terminal 1 and the COM terminal of the Thumbwheel Switch is used as the binary code.

Example of A7BS-206-PM

ModelSwitch Unit or
Connector
Common terminal
number
Terminals connected to
common
A7BSSwitch UnitC1248
Connector24567
Dial+ (0)
- (1)●
+ (2)●
- (3)●●
+ (4)●
- (5)●●
+ (6)●●
- (7)●●●
+ (8)●
- (9)●●

Note:

1.The solid dot ● indicates that the internal switch is ON.

2.Numbers enclosed in parentheses are the dial displays for the A7BS-206.

Recommended Products

61F-G[]N

Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL, WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Thumbwheel Switches FAQ