Page top

Lead Contents

FAQ02344 of Safety Relays FAQ

FAQ No. FAQ02344

Primary Contents

Question

For what purpose is the Safety Relay Unit provided with a feedback circuit?

Answer



For example, a feedback circuit is employed to detect welding of the contact point of the contactor which drives motors.

In this case, even if the contact point is welded, the Safety Relay Unit does not restart thanks to this circuit, thus ensuring safety.

However, be sure to use double contactors.

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Relays FAQ