Page top

Lead Contents

FAQ02379 of Safety Relays FAQ

FAQ No. FAQ02379

Primary Contents


What is the difference between the Safety Relay and the Safety Relay Unit?


Of course, safety circuits can be designed by using the Safety Relay. However, a reciprocal check of redundant circuits is required.

Meanwhile, the Safety Relay Unit is a block of circuits which combines the Safety Relay with other components in order for the safety circuit to be easily designed.

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Relays FAQ