Page top

Lead Contents

FAQ02115 of Basic Switches FAQ

FAQ No. FAQ02115

Primary Contents


What is the protective structure?


1.The protective structure protects the Switch from penetration by human bodies, solid foreign objects, dust, water, or oil. The degree of impermeability is increased by encasing or sealing the Switch so that it can be used in environments subject to dust, water, or oil.

2.The extent of this ability is expressed as the degree of protection. The degree is expressed with the protection characteristic code IP-[][].


IEC 60529: Defines degrees of protection against penetration of solid foreign objects and water.

JEM 1030: Defines degrees of protection against oil.

Recommended Products


Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.


Best-selling Basic Switch Boasting High Precision and Wide Variety


Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Basic Switches FAQ