Question
Which Basic Switches are suitable as door switches?
Answer
Hinge roller models are suitable. 
Example: Z-GW22 Basic Switch
        Sliding Door 1:
      
      
        Note:Push the actuator to approximately 70% to 100% of standard OT. 
        Note:When the door is closed, the slant of the dog is the first place that the actuator roller contacts.
        Sliding Door 2:
      
D-type, Q-type, and S-type Pushbutton Models can also be used for the actuator. 
      
        Note:Push the actuator to approximately 70% to 100% of the standard OT. 
        Double Door:
      
D-type, Q-type, and S-type Pushbutton Models can also be used for the actuator. 
      
        Note:Push the actuator to approximately 70% to 100% of the standard OT. 
        Closet:
      
      
        Note:The dog concept is the same as in Sliding Door 1, above.