Page top

Lead Contents

FAQ02049 of Limit Switches FAQ

FAQ No. FAQ02049

Primary Contents

Question

What is the difference between WL01CA2 Limit Switches and the WLCA2?

Answer



The "01" in WL01CA2 means that it is for microloads.

Microload Models (Refer to the following information when using the WL01CA2.)

Rated voltage (V)Resistive load (A)
125 VAC0.1
30 VDC

It is best to used the WL01CA2 in the range shown in the following figure.

Recommended load range5 to 30VDC
0.5 to 100 mA

Recommended Products

61F-G[]N

Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL, WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Limit Switches FAQ