Page top

Lead Contents

FAQ02990 of Limit Switches FAQ

FAQ No. FAQ02990

Primary Contents

Question

How do you calculate the operating force (OF) when changing the length of an adjustable roller lever in Limit Switches?

Answer



Use the following equation:

OF' = (OF x R)*/R'

*(OF x R): Fixed torque

Where OF is operating force, R is roller lever length, R' is the desired roller lever length, and OF' is operating force for the desired roller lever length.

For example, using the WLH12 Limit Switch with a roller lever length of 89 mm will result in the following OF':

(9.81 N x 38 mm)*/89 mm = Approx. 4.19N

*9.81 N: Standard OF
38 mm: Lever length for standard OF

In the above equation, the standard OF for a WLH12 with a roller lever length of 38 mm is 9.81 N (the OF listed in the datasheet), so the fixed torque is calculated as OF x R.

Dividing this by R' (89 mm in this example), which is the desired roller lever length, gives us the OF', which is the operating force for a Limit Switch with the desired roller lever length.

Recommended Products

61F-G[]N

Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL, WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Limit Switches FAQ