Page top

Lead Contents

FAQ03652 of Limit Switches FAQ

FAQ No. FAQ03652

Primary Contents

Question

How can I convert grams (g) for force in the operating characteristic to Newtons (N)?

Answer



Use the following formula to convert kgf (kilogram-force) to N (Newtons):

1 kgf = 9.80665 N

Therefore, 1 N is equivalent to approximately 102 g.
1 gf to 1/102 N

Example: 140 gf to 1.37 N

The unit for force in the operating characteristics for switches was previously expressed mainly in gram-force (g-f). Presently, however, the unit Newtons (N) is used under the new Japanese Measurement Law that went into force in 1992.

Recommended Products

61F-G[]N

Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL, WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Limit Switches FAQ