Page top

Lead Contents

FAQ02362 of Safety Limit Switches FAQ

FAQ No. FAQ02362

Primary Contents

Question

What is the difference between the Safety Limit Switches and the General Limit Switches?

Answer



The Safety Limit Switches are provided with a direct drive positive opening mechanism (positive actuation structure) with which welded portions are forcibly torn even if contact welding occurs, thus stopping a dangerous process (load) without fault and performing safe operation.

On the other hand, the General Limit Switches are not provided with the above mentioned mechanism. Therefore, if contact welding occurs, it keeps conduction state, and thus it cannot reliably stop dangerous process (load) and may perform dangerous operation.
For this reason, use the Safety Limit Switches in applications for safety purposes.

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Limit Switches FAQ