Page top

Lead Contents

FAQ01922 of Push Buttons / Indicator Lamps FAQ

FAQ No. FAQ01922

Primary Contents


The lamp does not light up even when Illuminating Type Push Button Switches are pushed.


Check the following points.

1. Is the polarity of the lamp is connected correctly?

2. Are the lamp's voltage specifications compatible with the applied voltage?

3. Terminals of the LED and the switch are separated and so it is necessary to connect them.

The terminal layout of the A16 is as follows.

Recommended Products


Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.


Best-selling Basic Switch Boasting High Precision and Wide Variety


Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Push Buttons / Indicator Lamps FAQ