Page top

Lead Contents

FAQ00542 of Temperature Controllers FAQ

FAQ No. FAQ00542

Primary Contents


How can ON/OFF control be used to maintain the temperature at 30 degree C?


Change the forward/reverse operation setting to forward operation. When the set point is set (i.e., 30°C), the output will be turned ON when the temperature rises above the set point, and OFF when it falls below the set point.

The output will turn ON when the temperature rises above the set point again.
(The point at which the output turns ON depends on the hysteresis.)

Applicable models: All models

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Temperature Controllers FAQ