Page top

Lead Contents

FAQ00560 of Temperature Controllers FAQ

FAQ No. FAQ00560

Primary Contents

Question

We need to perform heating control. With ON/OFF control, we need to increase the temperature of a 30°C oven to 100 °C. What settings are necessary?

Answer



Set direct/reverse operation to reverse operation.
(The factory default is for reverse operation.)

When you set the temperature (e.g., to 100 °C), the control output will turn ON when the temperature is below the set temperature and will turn OFF when it's above the set temperature.

If the temperature falls below the set temperature again, the output will turn ON again.

The point at which the output turns ON is also affected by the hysteresis setting.

Applicable Models: All Omron's Temperature Controllers

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Temperature Controllers FAQ