Page top

Lead Contents

FAQ00647 of Temperature Controllers FAQ

FAQ No. FAQ00647

Primary Contents

Question

We need to start a fan when the temperature rises and stop it when the temperature drops.

Answer



Set cooling control (direct operation).

Change the direct/reverse operation setting to direct operation.

For example, if you set the temperature (e.g., to 30 °C), the control output will turn ON when the temperature is above the set temperature and will turn OFF when it's below the set temperature.

If the temperature rises above the set temperature again, the output will turn ON again.
The point at which the output turns ON is also affected by the hysteresis setting.

Applicable Models: All Omron's Temperature Controllers

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Temperature Controllers FAQ