Page top

Lead Contents

FAQ02707 of Temperature Controllers FAQ

FAQ No. FAQ02707

Primary Contents

Question

What happens if the Temperature Sensor terminals are connected with the wrong polarity?

Answer



The measured temperature will not be displayed properly.

Thermocouples

If the polarity is connected in reverse, the Temperature Controllers will display a falling temperature when the temperature is actually rising.

Platinum Resistance Thermometers

If the polarity between A and B are reversed, "S.Err" will be displayed.
There is no polarity between B and B.

Make sure that the polarity and terminals are correctly connected.

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Temperature Controllers FAQ