Page top
Global
Global Navigation
Lead Contents
FAQ No. FAQ02710
Related Contents
Primary Contents
Question
What happens when the Controllers are in STOP mode before control is started?
Answer
There will be no control outputs.Set the RUN/STOP settings to RUN.
Outputs other than the control outputs (i.e., alarms) will be output.
A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals
A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.
Easy to Use and Easy to Read.
Local Navigation