Page top

Lead Contents

FAQ03633 of Temperature Controllers FAQ

FAQ No. FAQ03633

Primary Contents

Question

Can ES1B Infrared Thermosensors measure the temperature difference between two locations?

Answer



Yes. Refer to the following connections diagram.

Either a 12 VDC or 24 VDC power supply is required for ES1B.

To measure the temperature difference between two locations, use two isolated power supplies.

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Temperature Controllers FAQ