Page top

Lead Contents

FAQ02454 of Emergency Stop Switches FAQ

FAQ No. FAQ02454

Primary Contents


What are the restrictions when soldering A165E series Emergency Stop Switches?


There are the following restrictions.

1.Hand soldering: Use a 30-W soldering iron and complete soldering within 5 seconds.

2.Automatic soldering: Use dip soldering at 240°C and solder within 3 seconds.

3.Wait for one minute after soldering before exerting any external force on the solder.

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Emergency Stop Switches FAQ