Page top

Lead Contents

FAQ00768 of Digital Panel Indicators FAQ

FAQ No. FAQ00768

Primary Contents

Question

Which parameter should be set in order to display the K3NR Digital Panel Indicator's rotation speed?

Answer



When you want to display the rotation speed on the K3NR, the rotation speed will be expressed as:
Rotation speed (rpm) = Input frequency f (Hz) × 60 × α.

α = Prescale value

When displaying rpm with 2 pulses/rotation, make the following settings from the setup menu.

When 2 pulses are output/revolution, α = 1/N = 1/2 = 0.5 = 5.0000 × 10-1 m:

Reference: Calculating the Prescale Values

Equation variablesDisplay unitsPrescale value (a)
Speedrpm1/N
rps1/60N
Frequency (of input pulses)Hz1/60
kHz1/60000
Circumferential speedmm/s1000 πd/60N
cm/s100 πd/60N
m/sπd/60N
m/minπd/N
km/h0.06 πd/N

N: Number of pulses per rotation
πd: Circumference (units: m)

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Digital Panel Indicators FAQ