Page top

Lead Contents

FAQ00828 of Digital Panel Indicators FAQ

FAQ No. FAQ00828

Primary Contents

Question

What is Simple Average?

Answer



After taking n samples (measurements) this function displays their average value.

The display continues to show the previous value until n samples have been measured.

The displayed value is just the average of n samples, so the previous set of data is unrelated.

This function is useful when you want to lengthen the time between display updates.

Any number of samples can be selected for the simple average.

Note:The output responsive is slower when the readings are averaged.

Applicable models: K3HB-X, K3HB-V, K3HB-S, K3HB-H, K3HB-R, K3GN, K3MA-J, K3MA-F, and K3MA-L Digital Panel Indicators

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Digital Panel Indicators FAQ