Page top

Lead Contents

FAQ02937 of Digital Panel Indicators FAQ

FAQ No. FAQ02937

Primary Contents

Question

What kind of functions does the ThermoTools provide?

Answer



ThermoTools is a software utility for setting the parameters of Temperature Controllers and Digital Panel Indicators. Most of the parameters that are set using the front panel keys of these devices can be set with a personal computer using ThermoTools.

The utility also has an online data logging function for collecting data and a data log preview function for displaying data trends. However, because these are simplified functions, they are not suited for permanent connection.

Logged data can be saved either as a text file or a CSV file.

Applicable models: ESTT ThermoTools Support Software

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Digital Panel Indicators FAQ