Page top

Lead Contents

FAQ00186 of inverters FAQ

FAQ No. FAQ00186

Primary Contents

Question

We are running a three-phase 200 VAC induction motor on single-phase 100 VAC. Are there any Inverters with a function that boosts voltage from 100 VAC to 200 VAC?

Answer



There are 3G3EV Inverters that can accept a single-phase 100 VAC input. These models have built-in circuit that boosts the voltage from 100 VAC to 200 VAC.