Page top

Lead Contents

FAQ00675 of inverters FAQ

FAQ No. FAQ00675

Primary Contents


I am moving an Inverter from a location with a 50 Hz power supply frequency to another location with a 60 Hz power supply frequency. Are there any settings that need to be changed?


One of the features of the Inverter is that it will control operation at the same speed regardless of the power supply frequency.

The Inverter initially converts the input power supply to DC and then converts from the DC power supply back to AC, so differences in the power supply frequency have no effect on operation.