Page top

Lead Contents

FAQ01474 of inverters FAQ

FAQ No. FAQ01474

Primary Contents

Question

Can one Inverter be used to drive multiple motors?

Answer



Yes. Make the settings under the following condition:

Inverter rated current ≥ Motor rated current × 1.1 (at continuous operation)

Check whether the current is within the Inverter's overload capacity at maximum load. Electronic thermal relays cannot be used, so install a protective thermal relay for each motor.