Question
We are using an Inverter for speed control. How can we calculate the rotational speed of an induction motor?
Answer
Generally, the speed (N) of an induction motor is expressed by the following formula:
N = (120f/P) × (1 - S) (rpm)
f: Primary frequency
S: Slip
Example:
Where f = 60 Hz, P = 4 poles, and S = 3%,
N = ( (120 × 60) ⁄ 4) × (1 − 0.03) = 1,746 (rpm
 CS1W-NC[]71
CS1W-NC[]71 
                    
                  Decrease TCO with Simple Operation, Reduced Wiring, Batch Settings, and Batch Management
 CJ2
CJ2 
                    
                  Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Port.