Page top

Lead Contents

Weighing Indicator

K3HB-V

K3HB-V

An Ideal Indicator for OK/NG Judgements in Automated and Picking Machines, Measuring Factors such as Pressure, Load, Torque, and Weight Using Load Cell Signal Input.

Primary Contents



Application No.300

Load Measurement Control for Weighing Mixers



The K3HB-V Weighing Indicator is compatible with a load cell signal input. It measures and displays the load cell outputs for the measurement hopper of the weight mixer. The system then transfers the control output to the PLC to control the hopper.

Application No.301

Measurement of Remaining Liquid Gas



The system measures the weight of a tank that contains liquid gas with a load cell. The K3HB-V Weighing Indicator, which is compatible with a load cell signal input, converts and displays the value. You can select two display colors for operation judgments (green and red).

Application No.302

Pressure Control for Pressure Equipment



The system detects the pressure of a press fitting machine with a load cell. The load cell and the K3HB-V Weighing Indicator measure and display the values. Selectable green and red display colors enable judging the operation display at a glance. Control uses a set value.