Page top

Primary Contents



Application No.312

Temperature Monitoring for Power Generators and Motor Bearings



The E52 Temperature Sensor detects the generator or motor bearings. The two selectable display colors (green and red) let you see the operation status trends with the position meter on the K3HB-H Temperature Indicator. The communications output sends data to the computer to monitor for abnormal heat generation.

Application No.313

Temperature Indication Alarm for Molding Equipment



A Temperature Sensor detects the temperature status of the molding equipment. The application monitors the temperature with two selectable display colors (green and red) and a Temperature Indicator with a position meter. The system outputs an alarm when a temperature abnormality occurs.

Application No.314

Monitoring and Control of the Temperature Inside a Furnace



A Temperature Sensor detects the temperature in a furnace. The application controls and monitors according to the temperature and using the multilevel outputs of a Digital Temperature Indicator.

Application No.315

Measuring Temperature Changes in Copy Machine Rollers,



An ES1B Infrared Temperature Sensor detects the roller surface temperature. A Digital Temperature Indicator displays and measures the values. Effective use of the multilevel outputs according to temperature changes enables inspection of roller characteristics.

Application No.316

Monitoring Ship Engine Exhaust Temperatures



A Temperature Sensor detects the temperature at the engine exhaust pipe. A Temperature Indicator displays the values. The system outputs an alarm if there is a temperature abnormality.

Application No.317

Inspection Line for Gas Devices



In the inspection process for gas devices, an Infrared Sensor detects the gas combustion status. A Temperature Indicator displays the values. The system sends the temperature with linear output to a recorder to save the data.