Page top

A16

Pushbutton Switch (Detachable) (Lighted/Non-Lighted) (Cylindrical 16-dia.)

A16

Separate Construction with Cylindrical 16-dia. Body

(Unit: mm)

• The Dimension shows 2-switch outputs.
• The lamp terminal is also provided with non-lighted models.

Rectangular
A16[]-J
Solder terminals (tab terminals #110)

A16 Dimensions 2

See below for panel cutouts

Square
A16[]-A
Solder terminals (tab terminals #110)

A16 Dimensions 3

See below for panel cutouts

Round
A16[]-T
Solder terminals (tab terminals #110)

A16 Dimensions 4

See below for panel cutouts

• The Dimension shows 2-switch outputs.
• The lamp terminal is also provided with non-lighted models.
• A rectangular model is listed as an example.

Rectangular
A16[]-J[]-[]P
PCB terminals

A16 Dimensions 6

See below for panel cutouts

Rectangular
A16[]-J[]-T1
Voltage-reduction lighting, solder terminals (tab terminals #110)

A16 Dimensions 7

Rectangular
A16[]-J[]-2S, T1-2S, T2-2S
Screw-less Clamp

A16 Dimensions 8

Lamps

LED
A16-5D[]/-12D[]/-24D[]

A16 Dimensions 10

* The voltage display surface is the same color as the illumination color. The opposite surface is light gray.
   (For pure white, the entire surface is light gray.)

Incandescent Lamp
A16-5/-12/-24

A16 Dimensions 11

Accessories, Tools, and Components

Extractor
A3PJ-5080

A16 Dimensions 13

Legend Plates

A16ZJ-520[]

A16 Dimensions 15

A16ZA-520[]

A16 Dimensions 16

A16ZT-520[]

A16 Dimensions 17

Note: 1. The panel is 0.6 mm thick.
          2. The panel is made of the materials listed in the following table.

A16 Dimensions 18

Screw Fitting
A16Z-3004

A16 Dimensions 19

Panel Plugs (Black Resin)

Select the Plug that fits the panel design and mount from the front of the Panel. Panel cutouts are the same as those for Switches.
Protective structure: IP40
Color: Black

A16 Dimensions 20

Lock Ring

A16 Dimensions 21

Socket Unit Lamp Extractor
A16Z-5080

A16 Dimensions 22

Panel Cutouts

Solder Terminals and Screw-less Clamp Connectors

A16 Dimensions 24

Note:• Make sure the thickness of the mounting panel is between 0.5 and 3.2 mm. If, however, a Switch Guard or Dust
           Cover is used, the thickness of the mounting panel must be between 0.5 and 2 mm.
         • If the panel is to be finished with coating, etc., make sure that the panel meets the specified dimensions after
            coating.
         • Figures in parentheses are for Screw-less Clamp Connectors.

PCB Terminals

A16 Dimensions 25

Note:• Ensure that the variation in the distance between the centers of neighboring mounting holes is less than ±0.1
           mm.
         • Make sure the thickness of the mounting panel is between 0.5 and 3.2 mm. If, however, a Switch Guard or Dust
            Cover is used, the thickness of the mounting panel must be between 0.5 and 2 mm.
         • If the panel is to be finished with coating, etc., make sure that the panel meets the specified dimensions after
            coating.

Accessory Dimensions Mounted

Dimensions with Switch Guard Installed

Rectangular
A16ZJ-5050

A16 Dimensions 28

Note: This example is for when X is 4.5 mm.
          If X is not required, the Switches can be mounted with a minimum vertical installation pitch of 24 mm min.

Square
A16ZA-5050

A16 Dimensions 29

Note: This example is for when X is 4.5 mm.
          If X is not required, the Switches can be mounted with a minimum vertical installation pitch of 24 mm min.
          If PCB terminals are used, provide X must be 24 mm or larger.

Dust Covers

Rectangular
A16ZJ-5060

A16 Dimensions 31

Square
A16ZA-5060

A16 Dimensions 32

Round
A16ZT-5060

A16 Dimensions 33