Page top

F3SJ Series

Safety Light Curtain

F3SJ Series

Three versions available to meet your exact safety needs. All versions conform to the latest PLe/Safety Category 4 and SIL3 requirements.

[NEW] Implementation cost reduction with 1/2* the mounting time: Start with the "EASY type"

* Comparison with existing OMRON products.

The EASY type safety light curtain well is suited for straight forward on/off detection applications.

By carefully selecting the available functions, we have reduced man hours necessary for installation by approximately 1/2 when compared with existing OMRON models.

Reduced installation time means added savings to your project's budget, start with the EASY type.

F3SJ Series Features 5 F3SJ Series_Features1

Machine safety first, narrowed down to the simplest functions:

Upon detection of personnel, the machine stops. Simple yet very optimal.

F3SJ Series Features 6 F3SJ Series_Features2

1/2 the mounting time
Fixed response time makes calculation of the safety distance is easier.

Reduced wiring, quick mount brackets and easy-to-view alignment beams all add up to cost savings.
Additionally, with one fixed response time, it is know easier to calculate the safety distance.

F3SJ Series Features 7 F3SJ Series_Features3

Global Support

OMRON will support you through the our global network

F3SJ Series Features 8 F3SJ Series_Features4

Easy-to-view Diagnostics

These indicators enable you to intuitively know the status and cause of any error.
Allowing you faster installation while reducing machine down time.

[NEW] Fits any site, equipped with muting functions and series connection: Use the "BASIC type"

In addition to the simple functions inherited from the EASY type, such as global support, easy-to-view indicators, the BASIC type includes series connection and simple muting functions . This enables the BASIC type to satisfy installations that require multiple safety light curtains.

F3SJ Series Features 11 F3SJ Series_Features5

Up to three sets-connected in series

It is possible to connect up to three sets of safety light curtains in series. These sensors can be placed in a U-shaped or L-shaped pattern with a single power line, thus requiring less wiring.

F3SJ Series Features 12 F3SJ Series_Features6

Instant visibility of process trouble during muting

The BASIC type includes a muting function which temporarily disables the safety light curtain when a workpiece passes through. In the event of any trouble occurring, the error can be instantly recognized from the pattern of the LED indicators, allowing for a fast solution.

F3SJ Series Features 13 F3SJ Series_Features7

Functions inherited from the EASY type

Simple functions such as universal power voltage specification, easy-to-view diagnostics, a fixed response time have been inherited from the EASY type, As a result, expect reduced work-hours at each stage of use, from design and installation to operation.

Multi-functional for special applications such as finger protection: the "ADVANCED" type

The detection capability supports finger protection through use of 9 mm resolution. The ADVANCED type is equipped with various functions such as blanking, muting and the programing of warning zones. All settings can be done via an easy to use software tool. This Tool simplifies installations that were previously complicated, again our way of reducing cost and increasing productivity.

F3SJ Series Features 16 F3SJ Series_Features8

Tool for setting parameters and checking the system status

With the ADVANCED type (F3SJ-A) “SD Manager”, all parameters can be set and the system status can be checked with a personal computer. Complex settings are now simple to configure

F3SJ Series Features 17 F3SJ Series_Features9

Detection capability supports finger-protection

Even if the distance from the hazard is short, we have prepared a lineup that includes safety light curtains with a detection capability of 14 mm.

Versatile muting function possible

Equipped with partial muting that disables only the beams where a workpiece passes through, and position detection muting that disables the beams while detecting the position of a machine or robot.

F3SJ Series Features 19 F3SJ Series_Features10

Partial muting

F3SJ Series Features 20 F3SJ Series_Features11

Position detection muting

The blanking function disables specific beams of the Safety Light Curtain

If a part of the mechanical equipment is within the detection zone of the Safety Light Curtain, the relevant beams can be disabled. This is possible not only with non-moving parts but also with moving parts.

F3SJ Series Features 22 F3SJ Series_Features12

Fixed blanking

F3SJ Series Features 23 F3SJ Series_Features13

Floating blanking

Setting up a warning zone to prevent unnecessary stoppage

Under normal use, if an intrusion occurs in the safety zone, the machine will stop immediately. However, use of a warning zone will only notify the operator that an intrusion has occurred. This can be used to prevent carelessness resulting in machine stoppage on the part of the operator.

F3SJ Series Features 25 F3SJ Series_Features14

Dividing the zone between series-connected sensors

F3SJ Series Features 26 F3SJ Series_Features15

A single sensor zone can also be divided

Providing ease-of-use and ease-of-mounting through ingenuity

In pursuit of fast-easy mountable brackets *

* Sold separately

F3SJ Series Features 29 F3SJ Series_Features16-1

[Patent Pending]

OMRON has developed "quick mount" brackets which speed mounting to aluminum framing and reduce mounting time in half,when compared with existing models.<br/>This unique design allows for smooth horizontal movement, beam alignment is easy.

F3SJ Series Features 30 F3SJ Series_Features17

Top and bottom blue LEDs enabling beam alignment

F3SJ Series Features 31 F3SJ Series_Features16-2

Simple positional alignment can be done using the blue LEDs at the top (TOP) and bottom (BTM) of the emitter and receiver. With the blue LEDs ON, you can see at a glance that the beams' positions are correctly aligned.

F3SJ Series Features 32 F3SJ Series_Features18

Towards a more usable and installable safety light curtain.

Laser pointer used to easily align the beams *

* Sold separately

F3SJ Series Features 35 F3SJ Series_Features19

Use of the laser pointer allows simple alignment of the beams especially across long distances.
This saves approximately 60% of installation time.

F3SJ Series Features 36 F3SJ Series_Features20
F3SJ Series Features 37 F3SJ Series_Features21

Easy-to-understand diagnostics

F3SJ Series Features 38 F3SJ Series_Features16-3

Light curtain status can be immediately determined as the LED will light to indicate the status or possible error.

Communication error (EASY/BASIC type)

F3SJ Series Features 39 F3SJ Series_Features22

Input error (BASIC type)

F3SJ Series Features 40 F3SJ Series_Features23

Industry First! Error indication while muting is in progress.

F3SJ Series Features 41 F3SJ Series_Features24

The days of searching through user manuals to find the cause of certain muting errors are long gone. Now these errors and their causes can be well understood.

F3SJ Series Features 42 F3SJ Series_Features25

Providing multiple functions to cope with the various safety requirements

[NEW] Added the ENVIRONMENT RESISTANT type (F3SJ-B[][][][]P25-02TS) to the E3SJ series.

The coolant-resistant structure supports use in a severe work environment

F3SJ Series Features 45 F3SJ Series_Features26
F3SJ Series Features 46 F3SJ Series_Features27

Protects the sensor unit from direct exposure to the coolant.

The aluminum frame and transparent plate protect the sensor unit from direct exposure to the coolant. The cover protects the sensor's detection surface from collision with a workpiece, etc.

F3SJ Series Features 47 F3SJ Series_Features28

Protects the sensor from entry of the coolant that runs around the sensor.

The coolant-resistant H-NBR sponge used inside the cover protects the sensor from entry of the coolant that runs around the sensor.

Note:The sensor may be affected depending on the type of the cutting oil. Check the oil type before use.

Series connection up to 10 meters. Very convenient.

Sensors with protective heights of up to nearly 2.5 meters are available for applications that involve large-sized workpieces. And if you need to make changes in the future, you can always extend the protective height with series connections. Up to four sets, or 400 beams, can be series-connected, and with series connection cables up to 15 meters in length, applications can cover a wide area.

F3SJ Series Features 49 F3SJ Series_Features30

Tool for setting parameters and checking the system status

F3SJ Series Features 50 F3SJ Series_Features29-2

"SD Manager" PC Setting Support Software (For F3SJ-A)

F3SJ Series Features 51 F3SJ Series_Features31

All parameters can be set and the system status can be checked with a personal computer. In addition to making it easy to monitor the beam alignment, the ambient incident light intensity can be displayed in bar graph form for an easy check of the system status.

The "SD Manager" PC Setting Support Software helps reduce the time required for installing and troubleshooting the Safety Light Curtain.

Beam alignment is easier.

F3SJ Series Features 53 F3SJ Series_Features32

The incident light level can be displayed in a bar graph for each beam.

The ambient incident light intensity can be checked.

F3SJ Series Features 54 F3SJ Series_Features33

The incident light level when the light emission of the Safety Light Curtain is stopped is displayed in a bar graph.

The error log can be displayed.

F3SJ Series Features 55 F3SJ Series_Features34

The cause of the errors and countermeasures are both displayed.

Achieving muting function without a controller

F3SJ Series Features 56 F3SJ Series_Features35

The muting function temporarily disables the light curtain when an object must pass through the detection zone, such as when supplying a workpiece to your equipment. In the past, this function required a dedicated muting controller, but now it is built into the F3SJ. To use the muting function, purchase the Muting Key Cap (for F3SJ-B: F39-CN10 and for F3SJ-A: F39-CN6) (sold separately). The muting function is enabled simply by replacing the Unit's cap with this Key Cap. In addition, a muting sensor that determines the muting timing, as well as a muting lamp that notices the muting status to other operators, should be connected to the F3SJ.

Use example of a muting key cap for F3SJ-A

[Built-in muting function]

No controller required. Simply attach the Key Cap (sold separately) to the sensor.

F3SJ Series Features 58 F3SJ Series_Features36

Equipped with two muting functions

F3SJ Series Features 59 F3SJ Series_Features29-3

With F3SJ-A, the muting function temporarily disables the Safety Light Curtain when an object must pass through the detection zone, such as when supplying a workpiece to your equipment. "Partial muting," which further heightens the level of safety, and "position detection muting," which allows muting when the safety status can be determined by the position of a machine (such as a robot), have been newly added to the muting function.

Partial muting

F3SJ Series Features 60 F3SJ Series_Features37

Partial muting raises safety by muting only the beams of the Safety Light Curtain in the area where the workpiece passes through, while preventing muting in all other areas.

Position detection muting

F3SJ Series Features 61 F3SJ Series_Features38

This is used in applications where the workpiece is set in position each time by an operator, and then a turntable or positioning robot moves the workpiece to the area where the work is done. A limit switch or other means is used to detect when the robot is in a safe position, and muting is then applied.