(Unit: mm)
Liquid Leakage Sensor Amplifiers for Long-distance Wiring
about this Product Family
last update: November 1, 2018
(Unit: mm)
K7L-U/-UD/-UDP
K7L-UB/-UDB/-UDPB
F03-20
F03-20T
P2RF-08 (Round terminals can be used.)
Note: The applicable models of the K7L depend on the model of the Socket. If the correct Socket is not used, the K7L nameplate will be upside down.
P2RF-08-E
Note: The applicable models of the K7L depend on the model of the Socket. If the correct Socket is not used, the K7L nameplate will be upside down.
P2RF-08-PU
Note: The applicable models of the K7L depend on the model of the Socket. If the correct Socket is not used, the K7L nameplate will be upside down.
F03-16PS
F03-16PS-F
F03-26PS
* The Terminal Block is made of nylon 66. Mount the Terminal Block in locations not subject to liquid chemicals using M3 screws.
* Secure the Sockets with M3 screws at a torque of 0.78 to 1.18 N·m.
last update: November 1, 2018