Page top

R88M-K, R88D-KN[]-ML2

G5-series AC Servomotors/Servo Drives with Built-in MECHATROLINK-II Communications

R88M-K, R88D-KN[]-ML2

MECHATROLINK-II network communication modules are now available for the G5 series.

Data transfer using MECHATROLINK-II Communications:
All control data that can be interfaced between the Servo Driver and the Controller is transmitted using data communications. This enables maximizing the Servomotor performance without restricting the transmission performance of the control signals.

Having a communications module built into the Servo Driver significantly saves space in the control panel.