Page top

WS02-SGWC1 / CPLC1

FA Communications Software

WS02-SGWC1 / CPLC1

FA Communications Software Lets You Create Applications with Flexible, High-speed, and Direct Data Link Access to PLCs from Personal Computers.

System Requirements (CX-Compolet/SYSMAC Gateway)

Item Requirement
Operating system (OS)
Japanese or
English system *2
Microsoft Windows Server 2008 R2 (64bit*1)
Microsoft Windows Server 2012 (64bit*1)
Microsoft Windows Server 2012 R2 (64bit*1)
Microsoft Windows Server 2016 (64bit*1)
Microsoft Windows Server 2019 (64bit*1)
Microsoft Windows Server 2022 (64bit*1)
Microsoft Windows 7 SP1 (32bit/64bit*1)
Microsoft Windows 8.1 (32bit/64bit*1)
Microsoft Windows 10 (32bit/64bit*1)
Microsoft Windows 11 (64bit*1)
Personal compute Windows computers with Intel 32bit (x86) processor or 64bit (x64) -based processor
Hard disk At least 400 MB of available space

*1 This software runs on WOW64 (Windows-On-Windows 64). Refer to the sample program included with the product to run applications as 64-bit processes.
*2 We offer RHEL type.
 Please contact your OMRON sales representative for details.
Note 1: USB Port on the PC can not be shared between SYSMAC Gateway and CX-One in Windows Vista or higher.
Note 2: System requirements for Windows computers are the same as those recommended by Microsoft.
Note 3: The compatible functions of SYSMAC Compolet V2 are supported by Windows XP only.

Comparison between SYSMAC Gateway SDK and CX-Compolet

Yes: Supported, No: Not Supported

Communications
Method
Protocols Specifying
memory areas
SYSMAC Gateway SDK
(WS02-SGWC1S)
CX-Compolet+SYSMAC Gateway
(WS02-CPLC1)
Message
Communications
FINS Physical address Yes Yes
CIP Physical address Yes *1 Yes
Tag names No Yes
Tag Data Links
(EtherNet/IP)
CIP Physical address Yes *2 Yes
Tag names No Yes
Development languages C, C++ Visual Basic, C#

*1 Please use after understanding the CIP Communications Specifications.
*2 Data is transferred through the event memory.

Correspondence between Main PLC Models and Connected Networks

Yes: Supported, No: Not Supported

Personal computer RS-232C
PLC SYSWAY
(Host Link
C Mode)
SYSWAY-CV
(Host Link
FINS)
CompoWay/F
(master at
personal
computer)
Peripheral Bus
NX7/NJ1 (unit version 1.10 or later)*1
NJ5/NJ3 (unit version 1.03 or later)*2
NX5 (unit version 1.60 or later)*3
NX1 (unit version 1.30 or later)*4
NX1P (unit version 1.13 or later)*5
NY5[][]-1 (unit version 1.12 or later)*5
NX701-Z/NY5[][]-Z
(unit version 1.18 or later)*6
No No No No
CJ2 with EtherNet/IP functionality Yes Yes No Yes
(Peripheral Bus - CS/CJ)
CJ1 Yes Yes No Yes
(Peripheral Bus - CS/CJ)
CS1 Yes Yes No Yes
(Peripheral Bus - CS/CJ)
CP1 Yes *10 Yes *10 No Yes *10
(Peripheral Bus - CS/CJ)
C Series C200HX/HG/HE, CQM1H Yes No No Yes
(Peripheral Bus - C)
CPM1/CPM2 Yes No No Yes
(Peripheral Bus - C)
CVM1/CV Yes Yes No Yes
(Peripheral Bus - CV)
CompoWay/F Slaves, such as
Temperature Controllers
No No Yes No

Personal computer USB Ethernet (LAN) Controller Link
PLC FINS Ethernet (FINS) EtherNet/IP FINS
NX7/NJ1 (unit version 1.10 or later)*1
NJ5/NJ3 (unit version 1.03 or later)*2
NX5 (unit version 1.60 or later)*3
NX1 (unit version 1.30 or later)*4
NX1P (unit version 1.13 or later)*5
NY5[][]-1 (unit version 1.12 or later)*5
NX701-Z/NY5[][]-Z
(unit version 1.18 or later)*6
No No Yes *7 No
CJ2 with EtherNet/IP functionality Yes Yes Yes
(Specification
using tag names
is possible.)
Yes *8
CJ1 No Yes *8
(Communications Units
are not required for CJ1M
PLCs with Ethernet
functionality.)
Yes *8,*9 Yes *8
CS1 No Yes *8 Yes *8,*9 Yes *8
CP1 Yes Yes *11 No Yes *8
(CP1H only)
C Series C200HX/HG/HE, CQM1H No No No Yes *8
CPM1/CPM2 No No No No
CVM1/CV No Yes *8 No Yes *8
CompoWay/F Slaves, such as
Temperature Controllers
No No No No

Note: Including models whose production were/will be discontinued.
*1. To connect the NX701-1[][][]/NJ101-[][][][] Controller, CX-Compolet / SYSMAC Gateway version 1.70 or higher is
      required.
*2. To connect the NJ3/5 Controller, CX-Compolet / SYSMAC Gateway version 1.31 or higher is required.
*3. To connect the NX502-1[][][] Controller, CX-Compolet / SYSMAC Gateway version 1.81 or higher is required.
*4. To connect the NX1 Controller, CX-Compolet / SYSMAC Gateway version 1.72 or higher is required.
*5. To connect the NX1P/NY5[][]-1 Controller, CX-Compolet / SYSMAC Gateway version 1.71 or higer is required.
*6. To connect the NX701-Z[]00/NY5[][]-Z[]00 Controller, CX-Compolet / SYSMAC Gateway version 1.73 or higher is
      required.
*7. Tag data links between SYSMAC Gateway and the NJ/NX-series CPU Unit or Industrial PC Platform NY-series IPC
     Machine Controller can be created within the CJ-series specifications for variable with basic data type, array variable,
     and structure variable. SYSMAC Gateway memory allocation of structure variable is the same as the CJ-series.
     But, the tag data link with internal port of NY series is impossible.
*8. A separate Communications Unit is required.
*9. Specification using tag names is not possible.
*10. It cannot be used for CP1E E-type.
*11. The CP1W-CIF41 is required for the CP1H / CP1L other than CP1L-EM/EL. The CP1W-CIF41 version 2.0 or later is
       required for the CP1E N-type.
       It cannot be used for CP1E E-type.

Correspondence between supported OS and Development environment & CX-Compolet/SYSMAC Gateway

Supported CX-Compolet/SYSMAC Gateway
Supported OS Client Windows 7 SP1 (32bit) Ver.1.10 or higher
Windows 7 SP1 (64bit) Ver.1.20 or higher
Windows 8.1 (32bit/64bit) Ver.1.40 or higher
Windows 10 (32bit/64bit) Ver.1.70 or higher
Windows 11 (64bit) Ver.1.81 or higher
Server Windows Server 2008 R2 (64bit) Ver.1.20 or higher
Windows Server 2012/R2 (64bit) Ver.1.50 or higher
Windows Server 2016 (64bit) Ver.1.72 or higher
Windows Server 2019 (64bit) Ver.1.80 or higher
Windows Server 2022 (64bit) Ver.1.81 or higher
Development environment Visual Studio 2012 Ver.1.50 or higher
Visual Studio 2013 Ver.1.40 or higher
Visual Studio 2015 Ver.1.70 or higher
Visual Studio 2017 Ver.1.72 or higher
Visual Studio 2019 Ver.1.80 or higher
Visual Studio 2022 Ver.1.81 or higher

Note1: From SYSMAC Gateway version 1.80, the unit revision has been changed to revision 4. When EtherNet/IP tag
    data links are set for SYSMAC Gateway unit revision 1 to version 3, the settings need to be changed to revision
    4 with Network Configurator for EtherNet/IP.
   2: When EtherNet/IP tag data links are set to use SYSMAC Gateway unit revision 4 (version 1.80 or higher) as a
    node, Network Configurator for EtherNet/IP version 3.72 or higher is required.
    (Network Configurator for EtherNet/IP is included in
    · CX-Compolet WS02-CPLC1 version 1.80 or higher
    · SYSMAC Gateway WS02-SGWC1 version 1.80 or higher
   3: If you need to upgrade to the latest version of CX-Compolet, consult you OMRON representative.

Correspondence between supported OS & Connected Networks

Ethernet RS-232C USB Controller Link
Ethernet
(FINS)
EtherNet/IP PCI
Supported
OS
Client Windows 7 SP1 (32bit) Yes Yes Yes Yes Yes
Windows 7 SP1 (64bit) No
Windows 8.1 (32bit/64bit) Yes Yes Yes Yes No
Windows 10 (32bit/64bit) Yes Yes Yes Yes No
Windows 11 (64bit) Yes Yes Yes Yes No
Server Windows Server 2008 R2 (64bit) Yes Yes Yes Yes No
Windows Server 2012/R2 (64bit) Yes Yes Yes Yes No
Windows Server 2016 (64bit) Yes Yes Yes Yes No
Windows Server 2019 (64bit) Yes Yes Yes Yes No
Windows Server 2022 (64bit) Yes Yes Yes Yes No