Page top

XW5T-P

DIN Track Push-in Terminal Blocks

XW5T-P

Our Value Design Products Increase the Value of Your Control Panels. Push-in Plus Terminal Blocks to Downsize Control Panels and Save Work.

New Value For Control Panels

Control Panels: The Heart of Manufacturing Sites.
Evolution in control panels results in large evolution in production facilities.
And if control panel design, control panel manufacturing processes, and human interaction with them are innovated, control panel manufacturing becomes simpler and takes a leap forward.
OMRON will continue to achieve a control panel evolution and process innovation through many undertakings starting with the shared Value Design for Panel *1 concept for the specifications of products used in control panels.

XW5T-P Features 2

*1 Value Design for Panel
Our shared Value Design for Panel (herein after referred to as "Value Design") concept for the specifications of products used in control panels will create new value to our customer’s control panels.
Combining multiple products that share the Value Design concept will further increase the value provided to control panels.

OMRON Products from Terminal Blocks to Controllers Let You Efficiently Build Control Panels

Control panels can be downsized by using the many OMRON Controllers,
Power Supply, Relays, and other products that connect to the Terminal Blocks.
We will help you downsize control panels with OMRON control panel components that connect to terminal blocks.
We can also help you reduce terminal preparation and wiring work and reduce stock management work by maximizing the use of the components to unify tools and wires.

Everything from DIN Track Terminal Blocks to Controllers Available with Push-in Plus Terminal Blocks

XW5T-P Features 4

Push-In Plus Terminal Blocks for Easy Wiring

Just Insert Wires: No Tools Required Now you can use Push-In Plus terminal blocks to reduce the time and work involved in wiring.

Greatly Reduce Wiring Work with Push-In Plus Terminal Blocks

XW5T-P Features 6

Easy to Insert

OMRON’s Push-In Plus terminal blocks are as easy as inserting to an earphone jack. They help reduce the work load and improve wiring quality.

Held Firmly in Place

Even though less insertion force is required, the wires are held firmly in place. The advanced mechanism design technology and manufacturing technology produced a spring that ensures better workability and reliability.

XW5T-P Features 8

No Retightening Required

The retightening that is required for screw terminal blocks is not required for Push-in Plus terminal blocks.
Your work load is reduced not only when wiring, but also for inspections, delivery (shipping), and maintenance.

XW5T-P Features 9

Wiring Possible with Stranded Wires

You can insert wires with pin terminals or ferrules, or you can also insert solid wires or stranded wires.

When a stranded wire is used: 3 Steps.

XW5T-P Features 11

Screwdriver Held in Place to Free Both Your Hands

Optimized shape to hold the screwdriver was created by the resin parts and the spring.
Work goes smoothly when connecting stranded wires directly to the terminal because it’s easier to aim at the desired terminal.

XW5T-P Features 12

Safety

The structure provides finger protection so that your fingers never touch conductive parts.

Minimum Width of 3.5 mm to Help Downsize Control Panels

Terminal blocks are the most numerous, most space-eating components in control panels. OMRON has achieved the top class

*According to OMRON investigation in March 2017.

XW5T-P Features 15

Web Service That Helps Reduce Work in Selecting Terminal Blocks and Designing

• If you use OMRON’s website, you can easily select the Terminal Blocks to connect to the control panel
    components that you have selected.
• You can easily confirm the dimensions of the Terminal Blocks that you have selected.
• And you can easily create Terminal Block parts lists (BOMs) and marking formats.

XW5T-P Features 17

Take a Look Now! (www.ia.omron.com/solution/panel/)