faq00157- ... Answer  C120-LK201-EV1 cannot be used with C60P. Use 3G2C7-LK201-EV1 Host Link Units instead. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00157/
 
faq00225- ...orter of ON or OFF signal for sensor/pulse output > Length of one Programmable Controllers scan CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00225/
 
faq00242- ...urned on. Source Type is reversed, COM is plus, Current flows from Unit to Load when turned on. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00242/
 
faq00243- ...the power interruption will be detected, the CPU Unit will stop, and the outputs will turn OFF. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00243/
 
faq00245- ...ttery retains its charge. The contents of the DM Area will be backed up for at least 5 minutes. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00245/
 
faq00253- ...he Special I/O Units can be used on CPU Racks, Expansion Racks, and the SYSMAC BUS Slave Racks. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00253/
 
faq00254- ...ON. The RUN output will turn OFF when the CPU Units enter PROGRAM Mode or a fatal error occurs. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00254/
 
faq00258- ...eck Automatic generation method at [Driver] tab / Workstation node Address. Port Number = 9600. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00258/
 
faq00259- ...ble Controllers Setup to enter RUN Mode (set DM6600 to 0202) when power supplies are turned ON. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00259/
 
faq00264- ...oad on the ladder program is light. Others: Can be connected to a manual pulse generator (MPG). CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Por...
https://www.ia.omron.com/support/faq/answer/26/faq00264/