Page top

Lead Contents

FAQ00243 of Programmable Controllers FAQ

FAQ No. FAQ00243

Primary Contents

Question

What is the allowable momentary power interruption time for the CQM1-PA203/-PA206/-PA216/-PD026 Power Supply Units?

Answer



If the power is interrupted for less than 10 ms when using a CQM1-PA203/-PA206/-PA216, the Programmable Controller will continue to run normally.
If the power is interrupted for more than 25 ms, the power interruption will be detected, the CPU Unit will stop, and the outputs will turn OFF.
A power interruption that lasts more than 10 ms but less than 25 ms may or may not be detected. Operation in this case cannot be predicted.

If the power is interrupted for longer than 5 ms when using a CQM1-PD026, the power interruption will be detected, the CPU Unit will stop, and the outputs will turn OFF.