...rrecting PID constants when hunting occurs to eliminate hunting. Applicable Models: Thermac the K, and N Series * The N Series supports only mode 1. The step response method, a typical calcul...
...Question Can current outputs (4 to 20 mA DC) be used for the heating and cooling outputs of E5[]K Digital Controllers? Answer Current outputs can be used by adding E53-C3 Current output Uni...
...te 3 Note: 1.The [] in E5C4 model number indicates the type of input temperature sensor. It is "K" for the CA Thermocouple, "J" for the IC Thermocouple, and "P" for the Pt100 Resistance Therm...
...lect the Controller depending on the output type and any other conditions.) E5CN-[]L Series E5[]K Series Digital Controllers Temperature The temperature output of ES2-THB is the output of a P...
...n Support Software "ThermoTools"? Answer "ThermoTools" can be used with the E5[]R, E5[]N, E5[]K, E5ZN, and E5ZE Temperature Controllers; the K3N[] and K3GN Digital Panel Indicator; and the ...
...lect the Controller depending on the output type and any other conditions.) E5CN-[]L Series E5[]K Series Digital Controllers Temperature The temperature output of ES2-THB is the output of a P...
...he label "L" and the power supply for the sensing line is on the side of the CT with the label "K." Be sure that K and L are connected correctly (see Figure. 2). If the polarity is i...
...input terminal polarity. Cable: Terminal: The cable can be inserted in either direction. Either K or L can be connected to the input terminal of the Zero-phase Current Transformer. *Input Ter...
... polarity when using it with an AGD or K6EL Ground Fault Relay. Through-type: Separate-type: No K or L indication. Because it is used together with high-voltage equipment, it has K, ...
...ems, you can find your order, A~Z 0~9 from the initials of the format name. A B C D E F G H I J K L M N O P Q R S T U V W X Y Z 0 1 2 3 4 5 6 7 8 9 Those with the initials C for Automation Sy...